Dr. William C.Y. Lee serves as Chairman of LinkAir Communications, Inc., the
developer of LAS-CDMA-a new patented technology for wireless telecommunication
systems that significantly increases network capacity and improves quality of
service and network coverage. For 15 years, Dr. Lee was one of a team of
pioneers in developing advanced wireless technology—AMPS—for Bell Labs. During
that period he studied wave propagation in an anisotropic medium, antenna
theory, mobile radio propagation and systems, millimeter and optical wave
propagation, switching systems, and satellite communications. His UHF mobile
radio propagation model is known as the Lee Model.
He then joined the ITT Defense Communications Division, where he headed the
advanced mobile communications system. He studied artificial intelligence,
spread spectrum communications and frequency hopping scheme for military
applications. He won four patents in these fields. He was Vice President and
Chief Scientist during his subsequent tenure with Vodafone Airtouch—one of the
largest wireless carriers in the World, providing service to nearly 50 million
subscribers—Dr. Lee assisted in CDMA research and the initial trial of the
technology. The pioneer in personal communications network (PCN) technology, Dr.
Lee led PacTel’s PCS experimental trial, and under his leadership, the first
CDMA phone call was completed in Los Angeles in 1995.
Dr. Lee has been selected as an IEEE Fellow and has served as a member of
numerous Councils, including the California State Council on Science and
Technology, the US Council on Competitiveness, and was a former member of the
FCC Technical Advisory Council from 1999-2001. He has earned many prestigious
industry awards, including the IEEE VTS Avant Garde Award, the CTIA Award, the
CDMA Industry Achievement Award, the SATEC Award, a Bell Lab Award and, most
recently, the IEEE Third Millennium Medal Award. In 2001, Dr. Lee received the
Telecommunication Achievement award from Chinese Historical Society of America
and the Stuart Meyer Memorial award from IEEE Vehicular Technology Society.
Dr. Lee earned his Ph.D. in electrical engineering from Ohio State
University.
On UNIX, copy the Antconvert Program into the same directory as the ANET(r)
formatted antenna file(s) or find it at /usr/local/bin.
At UNIX prompt, type: Antconvert Filename
Once completed, a message will appear; filename 360 degrees horizontal 360
degrees vertical processed one antenna file.
Notes:
If antenna comes to you from ccmail or DOS based you will need to execute
the dos2unix command to convert the file once you have it on the UNIX
workstation. How can you tell if you need to run dos2unix? When using vi to edit
the file you will see ^M at the end of each line. Once you run dos2unix that
character should disappear. (i.e. dos2unix filename.ant filename)
Make sure the ANET(r) files begin with line "AA" before running the program.
If row "AA" is not the first line, it is probably not in ANET(r) format and the
antenna file will need to be modified.
If antennas are not in ANET(r) format, refer to ANET(r) data dictionary and
guidelines for converting ASCII antenna data to ANET(r). If there are only a few
antennas to be converted, they can be done manually using a tool such as
Microsoft Excel. If there are many antennas, it may be best to create a program
to run this conversion automatically.
Radio path clearance between antennas is an essential criterion for any point-to-point
communication system, and is one critical element of propagation conditions
of a mobile communication system. If a fairly large object exists in the radiation
path between two antennas, reduced received signal strength will occur because
the radio link relies increasingly on energy diffracted around the obstructing
object, rather than direct (line-of-sight) radiation. We can analyze this situation
quite easily using the concept of Fresnel zones.
Service providers are facing rapidly increasing pressure from zoning boards
to co-locate their base station antennas on the same tower structure as other
providers. Traditionally, these antenna installations have been vertically spaced
about 15 to 20 feet apart to ensure adequate antenna electrical isolation, intermodulation
and harmonic signal rejection, and resistance to receiver noise desensitization.
This note addresses the electrical coupling between horizontally and vertically
spaced antennas.
Abrasion Resistance:
Ability of material or cable to resist surface wear.
Absolute Delay:
The time interval or phase difference between transmission and reception of a signal.
Absolute Gain:
In simple language, absolute gain measures how much a device improves the power of a signal. The absolute gain of an antenna, for a given direction and polarization, is the ratio of (a) the power that would be required at the input of an ideal isotropic radiator to (b) the power actually supplied to the given antenna, to produce the same radiation intensity in the far-field region.
Accuracy Absence of error:
The extent to which a transmission or mathematical computation is error-free.
ANSI American National Standards Institute:
A standards-setting, non-government organization founded in 1918, which develops and publishes standards for transmission codes, protocols and high-level languages for "voluntary" use in the U.S.
Antenna:
A device for transmitting, receiving or transmitting and receiving signals. Antennas come in all shapes and sizes. Their shape depends on the frequency of the signal they are receiving or transmitting and the use to which their communications is being put.
Antenna Beam:
The radio frequency energy pattern emitted by an antenna.
Antenna Gain:
The ratio, usually expressed in decibels, of the power required at the input of a loss-free reference antenna to the power supplied to the input of the given antenna to produce, in a given direction, the same field strength, or the same irradiance at the same distance.
Antenna Lobe:
A picture showing an antenna’s radiation pattern. More technically: A three-dimensional radiation pattern of a directional antenna bounded by one or more cones of nulls.
Attenuation:
The decrease in power of a signal, light beam or lightwave, either absolutely or as a fraction of a reference value.
Attenuation Coefficient:
The rate at which average power decreases with distance.
B b
Base Station:
The fixed device a mobile radio transceiver (transmitter/ receiver) talks to.
Beam Tilt:
Generally refers to the angular tilt of the main lobe in the elevation pattern above or below 0 degrees elevation pattern above or below 0 degrees elevation. It must be referred to the free space pattern unless the actual vertical pattern approaches free space conditions (free from the ground reflection effects).
Beam Width
The angular width measured in degrees between the half power points (3 dB down from maximum) of the major lobe in either the elevation or azimuth radiation pattern.
Bluetooth:
A proposed wireless personal area network to standardize data synchronization between disparate PC and handheld wireless devices such as mobile phones, laptops, PDA's, etc.
Cable Assembly:
A completed cable that typically is terminated with connectors and plugs. It is ready to install.
Coaxial Cable:
A cable composed of an insulated central conducting wire wrapped in another cylindrical conducting wire. The whole thing is usually wrapped
I another insulating layer and an outer protective layer. A coaxial cable has great capacity to carry great quantities of information.
D d
Decibel (dB)
A convenient unit for expressing the ratio of the power gain or loss in an antenna or transmission line, or the relative intensity in the radiation pattern. dB gain = , where = output power and = input power. is the common logarithm. Decibels are convenient to use in figuring system gain
because they can be added and subtracted to obtain net gain.
Delay:
The wait time between two events, such as the time from when a signal is sent to the time it is received.
Digital:
In telecommunications, in recording or in computing, it is the use of a binary code to represent information.
Diode:
Devices that conduct electricity in one direction only.
Diplexer:
A device that permits parallel feeding of one antenna from two transmitters at the same or different frequencies without the transmitters interfering with each other.
Dipole:
Antenna fed from the center. (Name often applied to "rabbit ear" antenna.)
Directivity
The ratio of the maximum radiation intensity to the average radiation intensity. If the antenna and its feed system are lossless, the directivity is the same as the gain
Distortion:
The difference in values between two measurements of a signal - for example, between the transmitted and received signal. "Distortion" typically refers to analog signals.
Diversity (Polarization):
In radio communications, the strength of a signal can decrease for many reasons - heat, rain, fog, obstructions, etc. This is not good if the objective is to get reliable communications. One solution is to simultaneously receive two signals at different polarizations (i.e.; +45°/-45°). Since different polarizations respond differently to propagation problems, the likelihood is that at least one will get through well. This is called diversity receive polarization.
Duplexer:
A waveguide device designed to allow an antenna to be used for both transmission and reception simultaneously.
Earth Station:
The antenna and associated equipment used to receive and/or transmit telecommunications signals via satellite. ENTELEC:
Energy TELECommunications and electrical association, the oldest nationwide user group in telecommunications.
ESMR:
Enhanced Specialized Mobile Radio. An enhancement of SMR technology, allowing two-way radio service with the capability to provide wireless voice telephone service to compete against cellular.
F f
Ferrite:
A type of ceramic material having magnetic properties and consisting of a crystalline structure of ferric oxide and one or more metallic oxides, such as those of nickel or zinc.
Filter:
A device which transmits a selected range of energy. It is used to suppress unwanted frequencies or noise, or to separate channels in communications circuits.
Flame Resistant:
Insulated wire Which has been chemically treated so it will not aid the spread of flames.
Free Space
In space clear of the earth or other bodies so that radiation is propagated on a direct path only. Antenna patterns generally are shown as free space patterns.
Frequency:
The rate at which an electrical current alternates, usually measured in Hertz per second.
Gain
Often referred to as power gain, it is the ratio of the maximum radiation in a given direction to that of a reference antenna in the same direction for equal power input. Gain differs from directivity in that it takes into consideration the losses in the antenna as well as a specified direction, angle, or plane of the radiation pattern. In two-way radio, gain generally is referred to a half-wave dipole in free space at 0 degrees elevation in the elevation pattern.
Gigahertz GHz:
A measurement of the frequency of a signal equivalent to one billion cycles per second, or one thousand million cycles per second.
GSM:
Groupe Special Mobile, now known as Global System for Mobile Communications. It is the standard digital cellular phone service in Europe, Japan, Australia and elsewhere - a total of 85 countries around the world.
H h
Half-Wave Dipole (dB)
A half wavelength antenna, center fed so as to have equal current distribution in both halves. Mounted vertically, it has a doughnut shaped pattern, circular in the horizontal plane. It is an antenna that can be constructed. It has some inherent losses. When used as a gain reference, the half-wave dipole has a power gain of 0 dB.
Hertz Hz:
A measurement of frequency in cycles per second. A hertz is one cycle per second.
ISO 9000 Series:
The ISO 9000 Series, published in 1987, outlines the requirements for the quality system of an organization. It is a set of generic standards that provide quality assurance requirements and quality management guidance.
ISO 9001:
ISO 9001 is a rigorous international quality standard covering a company's research and development, design, production, installation and service procedures.
ISO 9002:
ISO9002 covers manufacturing and installation only. See ISO 9000 Series.
Isotropic (dBi).
Generally refers to a theoretical antenna having a spherical radiation pattern with equal gain in all directions. Used as a standard or reference level for measurement of gain - especially at microwave frequencies. When used as a gain reference, the isotropic antenna has a power gain of 0 dBi.
J j
Jumper :
A coaxial cable assembly used to connect components of an RF System. (i.e.; antenna to feeder jumper)
L l
"Lossless" Half-Wave Dipole (dBd)
Another theoretical antenna, it has a directivity and power gain of 2.15 dB over an isotropic. When used as a gain reference, the "lossless" half-wave dipole has a power gain of 0dBd.
Megahertz (MHz):
A unit of frequency denoting one million hertz, or one million cycles per second.
Mobile Cellular Phone:
The cellular handset unit used for voice and data communications.
Mobile Phone:
One term for a cellular phone. There are four main types of cellular phones - mobile (also called a car phone), tranportable, portable and personal.
Monopole:
A slender self-supporting tower on which wireless antennas can be placed.
Multiplexer:
Electronic equipment which allows two or more signals to pass over one communications circuit.
N n
Noise Figure NF:
The ratio (in dB) between the signal-to-noise ratio applied to the input of the microwave component and the signal-to-noise ratio measured at its output.
Non-loaded Lines:
Cable pairs or transmission lines with no added inductive loading coils. In short, straight, raw copper pairs. Null Fill:
OEM:
Original Equipment Manufacturer. The maker of equipment marketed by another vendor.
P p
PCIA:
Personal Communications Industry Association.
PCS:
Personal Communications Service: A new, lower powered, higher-frequency competitive technology to cellular. PCS operates in the 1.5 to 1.8 GHz range.
Phase:
The relationship between a signal and its horizontal axis, also called zero-crossing point.
Ping Pong:
A disruptive phenomenon that occurs in digital cellular networks when the cell phone repeatedly reselects two cell sites of approximately equal strength.
Polarization
The orientation of the electric field vector (E) for maximum radiation. If the long dimension of the radiator is vertical, generally the polarization is vertical; if horizontal, the polarization likewise horizontal. Most two-way radio antennas are vertically polarized.
Power Rating
The input power to the antenna terminals that the antenna can safely handle and deliver its rated performance. Generally, it is limited to the power handling capacity of the feed line.
Rack:
An equipment rack, typically made of aluminum or steel, onto which equipment is mounted.
Radiation Pattern
A graphical representation of power radiation of an antenna usually shown for the two principal planes, azimuth and elevation. The radiation pattern of an antenna is usually measured in the far field which is generally considered to be beyond the distance of 2 times D2 divided by the wavelength (where D is the radiating length of the antenna).
Radio RF:
System of communication employing electromagnetic waves operating between 10 kHz and 3 MHz, propagated through free space without guide (wire or cable). Because of their varying characteristics, radio waves of different lengths are employed for different purposes and are usually identified by their frequency. The shortest waves are the highest frequency, or numbers of cycles per second; the longest waves have the lowest frequency, or fewest cycles per second.
Radio Frequency:
That group of electromagnetic energy whose wavelengths are between the audio and the light range. Electromagnetic waves transmitted usually are between 500 KHz and 300 GHz.
Radome:
A plastic cover for a microwave antenna. It protects the antenna from awful weather, but has little effect on the radiation pattern of the antenna.
Real Time:
A voice telephone conversation is conducted in real time. That is, there is no perceived delay in the transmission of the voice message or in the response to it.
Receive Only RO:
Describing operation of a device that can receive transmissions but cannot transmit.
Receiver:
Any device which receives a transmission signal. Or, any portion of a telecommunications device which decodes an encoded signal into its desired form.
Reflections:
RF waves can reflect off of hills, buildings, moving cars, the atmosphere and basically almost anything in the RF transmission environment. Reflections may vary in phase, polarization and strength from the original wave. They are what allow radio waves to reach their targets around corners, buildings, etc. RF transmissions bend around objects as a result of reflections.
Reliability:
A measure of how dependable a system is once you actually use it.
S s
SMR:
Specialized Mobile Radio. Also known as TMR (Trunk Mobile Radio). A two-way radio telephony service making use of macrocells covering an area of up to 50 miles in diameter.
SMS:
Short Message Service. A means to send or receive short, alphanumeric messages to or from mobile telephones.
TDMA:
Time Division Multiple Access. One of several technologies used to separate multiple conversation transmissions over a finite frequency allocation of through-the-air bandwidth.
Telecommunications:
The art and science of "communicating" over a distance by telephone, telegraph and radio.
Terahertz THz:
A unit denoting one trillion (10 to the 12th) hertz.
3G:
Refers to Third Generation wireless technologies that will transmit data as well as voice.
Transceiver:
Any device that transmits and receives.
Trunk:
A communication line between two switching systems.
U u
U-NII:
Unlicensed-National Information Infrastructure. A group of three frequency bands, each of 100 MHz in the 5GHz band, set aside by the FCC in January 1997 for support of a projected family of high-speed, low-power, wireless voice and data devices.
UMTS:
Universal Mobile Telecommunications System. The technology envisioned for the next generation of Global System for Mobile Communications. UMTS is intended to support data transfer rates of 144 Kbps to 2 Mbps in support of mobile acces to multimedia Internet applications.
V v
VSWR
Voltage standing wave ratio is the ratio of the maximum to the minimum values of voltage (or current) in the standing wave pattern at the antenna terminals. A standing wave is produced when the antenna (load) impedance differs from the characteristic impedance of the transmission line.
Wavelength ()
The ratio of the velocity of the wave to the frequency of the current causing the wave. [Formula: Wavelength times feet = 984 x 300m divided by frequency (MHz)] Wavelength at higher frequencies is more conveniently expressed in inches: [Formula: Wavelength times inches = 11808 x 300m divided by frequency (MHz)]
WCA:
Wireless Communications Service. Licensed spectrum in the 2.3 GHz band. May be used for wireless broadband Internet service.
WCS:
Wireless Communications Service. Occupies 30 MHz of spectrum in the frequency rang eof 2.305-2.360 GHz. Also known worldwide as the Industrial, Scientific and Medical band (ISM).
Lightning happens! While it can be a spectacular phenomenon to witness, it
can also cause damage to property, structures, and even be fatal to human life
if not respected. Without a doubt, expenses from lightning damage can be substantial—especially
for companies whose equipment is installed on tall structures (since lightning
tends to strike taller objects). The wireless antenna industry is particularly
at risk with its multitude of towers.
Some customers may want to paint their antenna radomes to match a specific
color scheme. This Andrew Tech Note lays out some good practices to consider
when painting Base Station Antenna radomes, although it is not intended to
replace the manufacturer's instructions. Please consult the paint manufacturer
for product information, specific equipment, recommended mixing methods, and
application instructions. Although we refer to specific products, we do not
endorse one manufacturer over another; several products can be used
successfully.
Paint One readily available, low VOC paint is Sherwin
Williams Polane HS Plus Polyurethane Enamel. Sherwin Williams recommends that
catalyst V66V55 be used with this paint. Vinyl wash primer may be used, but is
not necessary for this paint on nonmetallic surfaces.
Be careful when selecting paints: the paint you choose cannot contain
metallic particles, high levels of carbon, or conductive dyes. Paint must be RF
transparent and UV resistant. (Note: Sherwin Williams Polane Silver paint
contains metallic particles, so it should not be used.)
Helpful Hints to Consider Before Painting Antenna Materials
Antenna Materials The radome of Andrew PCS/DCS antennas
is made of acrylic/PVC plastic; the end caps and back panel are made of
aluminum.
The radome of Andrew panel antennas is made of ABS plastic; the back panel is
made of aluminum.
Surface Preparation Remove old layers of paint or other
surface contamination before painting. Water with a mild detergent,
industrial-grade isopropyl alcohol, or acetone (highly flammable) are good, low
VOC cleaners.
On smooth surfaces, such as PCS antenna radomes, we recommend light sanding
with 400 grit or higher sandpaper. After sanding, always clean the surface with
isopropyl alcohol or other cleaner to remove grit and dust.
General
Precautions
All paints and cleaners must be compatible with the radome material and must
be RF transparent.
All connectors and labels should be masked before painting.
DC grounding must be maintained during painting.
All drain holes and other ventilation holes must remain open and clear
during painting.
Technical Support
If you have questions or concerns about the operation of your Andrew Base
Station Antenna or if you are planning the installation of a new system, Andrew
can help. We encourage you to contact our Applications Engineering Department by
calling toll-free 1-800-676-5342 in the United States and Canada. Outside the
U.S. and Canada, you can reach the Applications Engineering Department by
calling 1-214-631-0310.
To ensure published performance of our products, all families of Andrew base
station antennas are tested and must successfully complete rigorous environmental
performance tests per IEC 60068–2 standards or ETS 300 019–1–4 class 4.1E conditions
prior to release for manufacturing.
As cellular systems become more sophisticated and components such as duplexers,
diplexers and dual-band/tri-band/multi-port antennas are more common, questions
often arise about how to handle ports that are not used at the time of initial
installation.
A system return loss sweep is the most common method of testing antenna and
cable performance. The results of these measurements need to be analyzed carefully
as each site is configured differently. These differences can drastically affect
system return loss characteristics. Cable length, cable diameter, cable insertion
loss characteristics, connectors, jumper cables and other components all influence
the measured system return loss values. A reasonable system sweep should measure
between –14 dB to –20 dB, depending upon the configuration. Site return loss
specifications and base station equipment alarm thresholds should be set accordingly.
A torque wrench is recommended when installing DIN 7-16 connector jumper
cables. The correct amount of connector torque greatly minimizes the chances
of PIM generation and/or water leakage.